2018-12-17 6:00 AM
2018-12-20 5:18 AM
Hello Zhang,
For ST25DV64k, Cs is also 28.5pF. You thus just need to design/use an antenna which inductance around 4.5uH, there is not need for additional resistor.
Have a nice day
Denis
2018-12-17 6:07 AM
Probably to disconnect the antenna easily with removing the resistor.
2018-12-18 12:11 AM
Hello Zhang,
I am really sorry but I don't understand your point.
Denis
2018-12-18 4:20 PM
I hope to design R and L value of the st25dv64 external antenna, not internal PCB antenna by tool. In the AN2972 document, “2.3 Basic equations “ , I don’t know Rs and Cs. So I could not designed antenna of st25dv64. In the other document about M24LR64, Cs is 28.5pF, Rs is 5Ohm. By those parameters, I would calculate R and L of M24LR64 antenna, Ra is 5Ohm , L is 4.5uH. I hope to test real resistor between AC0 and AC1of St25dv64 with the X-NUCLEO-NFC04A1. The test resistor value is1Ohm, not 5Ohm or2.5Ohm. Thanks!
2018-12-18 4:22 PM
Hi,
Thanks for your reply. Which resistor to remove?
Thanks!
BR
zhang
2018-12-20 5:18 AM
Hello Zhang,
For ST25DV64k, Cs is also 28.5pF. You thus just need to design/use an antenna which inductance around 4.5uH, there is not need for additional resistor.
Have a nice day
Denis
2018-12-20 3:52 PM
Hello Denis
Thanks.It is important for me.
Have a nice day!
BR,
zhang
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.