2019-09-25 6:51 AM
The autotuning algorithm implemented in the app reader, is an external routine? I mean, the IC ST25RU3993 by itself can not tune an antenna. I guess that we need to implement some algorithm making a sweep and checking the reflected power, and then finally set the 3 values for the tunning capacitors.
Solved! Go to Solution.
2019-09-26 4:28 AM
Hi, the tuning algorithms are all completly implemented in the FW, the "Reader Suite" application simple call them in the FW. You find all the necessary implementation in the file "tuner.c". The 4 algorithms are implemented in the following functions "tunerOneHillClimb" -> FAST, "tunerDuplicatedOneHillClimb" -> VERYFAST, "tunerMultiHillClimb" -> SLOW and "tunerEnhancedMultiHillClimb" -> MEDIUM.
Hope this answers your question, if you have further questions let me know.
BR Nick
2019-09-26 2:39 AM
Hello, yes correct. The carrier cancelation circuite is a external HW component that is controlled by an MCU (The same MCU that controlls also the ST25RU3993). As an example how this could look like in HW and how it is used in FW please have a look into the EVAL board schematic and the EVAL board FW. Both could be found on www.st.com
Best Regards
2019-09-26 4:10 AM
Dear Nick, Hi. I understand. But I mean that the search algorithms (OneHillClimb, MultiHillClimb, DuplicatedFastHillClimb, and EnhancedMultiHillClimb) I guess that the Appreader app implements them. I could not see this algorithms into the fw side.
Regards
2019-09-26 4:28 AM
Hi, the tuning algorithms are all completly implemented in the FW, the "Reader Suite" application simple call them in the FW. You find all the necessary implementation in the file "tuner.c". The 4 algorithms are implemented in the following functions "tunerOneHillClimb" -> FAST, "tunerDuplicatedOneHillClimb" -> VERYFAST, "tunerMultiHillClimb" -> SLOW and "tunerEnhancedMultiHillClimb" -> MEDIUM.
Hope this answers your question, if you have further questions let me know.
BR Nick
2019-09-26 7:57 AM
Dear Nick,
I am sorry. I could find them before.
Thank you so much.
Best Regards
Franco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.