2025-08-15 8:23 PM
Hi,
I am using a ST25R3920 to emulate a type 2 tag. I have got the Read part working and I am able to send 16 bytes of data in response to 0x30 and confirm the data on a phone. But when the phone tries to write data using 0xA2, I am unable to send the 4 bit Ack (0xA) response that is acceptable for the phone which throws a write error. On probing the modulation using an oscilloscope, I noticed that the ST25 is sending
start 0101 0000 parity
instead of
start 0101 parity
Here is my send sequence:
Clear FIFO
Set ntx = 0, nbtx = 4 (to send only 4 bits)
Load FIFO with 0xA
Transmit without CRC
Is it possible to send 4 bit frames in card emulation mode with this chip to support type 2 communication?
Solved! Go to Solution.
2025-08-29 3:46 PM
I think I figured out the issue. If automatic anti-collision (d_106_ac_a) is disabled before sending, then only the 4 bits are sent as expected. Maybe this was supposed to be disabled when the tag reaches active state? I apologize if I had missed this in the RFAL.
Thanks for your help!
2025-08-20 9:05 AM
Hi,
Please try using no_tx_par=1, even though footnote says differently. This option was not fully verified but you have a good chance that it works well for your use case.
If you run into issues with it, then please let me also know.
BR, Ulysses
2025-08-20 1:26 PM
I have already tried no_tx_par=1 without any success, still sends 8 bits. Since stream mode is also not supported in card emulation, is there any other option or is the chip not capable of sending 4 bit frames?
2025-08-21 2:39 AM
Hi,
I know for sure that ST25R3918 is capable of doing these 4 bit responses. ST25R3920 is using same logic and is identical in this respect. Or are you using ST25R3920B?
I have some traces showing r05h:0x80, r22h:0x00, r23h:0x04, FIFO getting 0xFA and transmission using C5 causing 4 bits being sent.
BR, Ulysses
2025-08-21 10:43 AM
I am using 3920, not the B. Are your traces from reader or card emulation mode, because I have seen 4 bit frames in reader mode.
Here is my initial configuration, in case I am missing something:
Set default
REG_OP_CONTROL = en | rx_en | en_fd_auto_efd
REG_MODE = targ | om_targ_nfca | nfc_ar_off
REG_PASSIVE_TARGET = 0
REG_AUX = nfc_id_7bytes
Load PT_Memory
Go to sense
2025-08-22 1:31 AM - edited 2025-08-22 4:58 AM
Hi,
the traces I am referring are from CE mode. In these the ST25R3918 emulates a T2T including NDEF read-out and everything. These 4-bit responses are then issued once the pta_state has moved to ACTIVE/ACTIVE*.
I recommend to start with such a scenario - perform the Anticollision using automatic responses (d_106_ac_a=0) and then perform commands for exchanging 4 bit responses.
Ulysses
2025-08-25 2:42 AM
Hi,
The ST25R3920 supports T3T and T4T card emulation. T2T card emulation is not an officially supported feature.
The following is a trace from the logic analyzer, showing a 4-bit acknowledgment being sent in card emulation mode:
Some devices, such as the Flipper Zero, emulate T2T tags. Refer to the Flipper Zero firmware source code for more details.
Rgds
BT
2025-08-27 5:23 PM
I was using the automatic anti collision and once the tag reached ACTIVE state, the reader sends a write command and the tag sends a 4-bit 0xA in response. The reader in this case is also a ST25R3920 and it generates interrupts for hard framing error and no response timeout after a start of receive. It never moves to end of receive when the tag tries to send a 4-bit frame using TX without CRC. Since the oscope confirmed that the tag is sending 8 bits instead of 4 bits, the reader times out expecting the CRC?
2025-08-27 5:34 PM
Hi @Brian TIDAL
Thanks for pointing to the Flipper Zero code. It looks like it uses transparent mode to send 4 bit short frames.
I am sending the same sequence of commands you have shown in your logic analyzer trace. But the chip sends 8 bits instead of 4. Do you have a trace of the actual load modulated signal or the data received at the reader end to confirm it actually sends 4 bits?
If T2T is not officially supported, does it mean the 3920 is not capable of sending 4 bit frames except in transparent mode?
2025-08-28 3:47 AM
Hi,
I had a chat with Brian as well: We know that chip is able to send 4bit ACK/NACK and we are using it in one of our dedicated demos to emulate a T2T. It is not an official feature and there might be issues in some corner cases - maybe you are running into one.
Can you please share a scope shot of the modulation, that you are seeing, please?
In our opinion it would be best if you would have a working reference. We will try to work on a small proof showing such frames work but this may take a few days. We were considering such based on ST25NFC Lib, so X-CUBE-NFC06 + NUCLEO-L474. Is this something you have at hand? If not, please share what you have.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.