2025-05-30 2:12 AM
"I modified the card emulation routine in codebase STEVAL-25R3916B_V2.1.0 by changing RFAL_ISODEP_CMD_RATS to 0x60. After receiving 0x60, the authentication handshake is initiated. The problem arises when using rfalStartTransceive(&ctx) with the following configuration:
ctx.flags = RFAL_TXRX_FLAGS_CRC_TX_MANUAL |
RFAL_TXRX_FLAGS_CRC_RX_KEEP |
RFAL_TXRX_FLAGS_NFCIP1_OFF |
RFAL_TXRX_FLAGS_AGC_ON |
RFAL_TXRX_FLAGS_PAR_RX_KEEP |
RFAL_TXRX_FLAGS_PAR_TX_NONE;Why is the RFAL layer automatically adding parity bits despite PAR_TX_NONE being set?"
Solved! Go to Solution.
2025-06-02 4:44 AM
Hi,
the DS should have a note "1. Supported in reader modes only, not supported in card emulation modes."
RFAL should probably check and refuse such unsupported configuration.
BR, Ulysses
2025-06-02 4:44 AM
Hi,
the DS should have a note "1. Supported in reader modes only, not supported in card emulation modes."
RFAL should probably check and refuse such unsupported configuration.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.