2025-08-07 9:58 AM
Hi everyone,
I'd like to use the ST25R3916B device for a very low-power device. I downloaded the X-CUBE-NFC6 library version 3.0.0, and I don't see an example of calling rfalLowPowerModeStart().
I saw earlier that someone managed to find it in version 1.0.0, but I can't find it anywhere.
Could someone help me? Or provide the library in this version, or an example of using this function in the latest version?
By the way: Why isn't this functionality included in the current examples? I think it's a very useful feature.
Best regards to everyone :)
Solved! Go to Solution.
2025-08-20 7:14 AM
Hi,
not sure what you want to achieve using rfalLowPowerModeStart(). It will put the device into a low power state not reacting to any events on the NFC antenna. The function is there, you can use it e.g. after having stopped the discovery (rfalNfcDeactivate(RFAL_NFC_DEACTIVATE_IDLE)).
BR, Ulysses
2025-08-20 7:14 AM
Hi,
not sure what you want to achieve using rfalLowPowerModeStart(). It will put the device into a low power state not reacting to any events on the NFC antenna. The function is there, you can use it e.g. after having stopped the discovery (rfalNfcDeactivate(RFAL_NFC_DEACTIVATE_IDLE)).
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.