2025-10-20 6:44 AM
Hello, I have a problem after updating the system to Android 16. Before, everything was great. I have a custom application to work with ST25DV04KC. Now, the NFC service crashes before connection, and the system app opens NDEEF. Only on the first "tap," after turning NFC on/off, the connection is correct. Is there any workaround before they change it in Android? Thanks for any help.
Solved! Go to Solution.
2025-12-09 1:48 AM
Hello
Just to summarize, but to be sure all of us have the information, Samsung provides fix for mobiles, i have updated my S24 with update, works fine now without App changes.
BR,FB
2025-10-24 2:18 AM
I also have a problem after updating to Android 16. I have a working app with ST25DVCTag and Android <= 15, but with Android 16 I must manually restart toggle NFC in the device before the re-estarting the app.
2025-10-28 2:51 AM
Hi @JordiCasadevall @DanZak ,
Which model of Android phone do you use (Manufacturer, Model)?
"I have a custom application to work with ST25DV04KC": Is this custom App based on ST25 SDK? If yes, which version?
Can you read the tag with the ST25 NFC Tap App? With other NFC app such TagInfo?
Rgds
BT
2025-10-28 3:43 AM
Hi BT,
with TagInfo app, ST25 NFC app and our developed app: After a tag is discovered and then lost, it does not work unless I toggle NFC in the mobile or I wait for a 60/70 seconds aprox.
My Android is a Samsung Galaxy S23 upgraded to One UI Version 8.0 Android 16.
With Android 15 everything perfectly without having to wait between tag lost and new tag discovering.
The App is based on ST25 SDK v1.10.0 and st25_android_reader_interface-1.0.10-release. Tried with S25 SDK v1.13.0 but is compiled with JDK 21 (class file major version 65). We need JDK 17 (class file major version 61) since it is the max stable version fully supported by Android and React Native, and Android Gradle Plugin.
I look forward to your response, thank you,
Jordi
2025-10-30 7:12 AM
Hi @JordiCasadevall @DanZak ,
I did some tests on Pixel8/Android16 and Samsung S25/Android16 and not seen direct issue....
We talk also about some version and JDK, on my side i have JDK17, you can find on st.com materials build with JDK17....
Please see : STSW-ST25001 | Product - STMicroelectronics
At the end of page, you have an apk + src of this apk. With sources you can find in the android project, both ST25SDK + ReaderInterface at version : st25sdk-1.13.0, st25_android_reader_interface-1.0.13-release.
Can you please advise if theses artefacts are usable on your side and able to allow progress to be made on the problems?
Rgds, FB
2025-10-30 8:27 AM
JDK17 issue solved, from https://www.st.com/en/embedded-software/stsw-st25001.html I found libraries compiled with Major 52 (ok for jdk 17)
Previously I downloaded from https://www.st.com/en/embedded-software/stsw-st25sdk001.html with Major 65 (jdk 21)
So I was able to compile my app with ST25 1.13.0 and st25_android_reader_interace-1.0.13, good.
But the NFC issue with my Samsung S23 updated to Android 16 continues with our app and also your app "ST25 NFC Tap", while with Android 15 everything worked fine.
The problem with ST25 and some devices with Android 16 has also been reported here: https://forum.developer.samsung.com/t/one-ui-v8-update-causing-nfc-readermode-to-crash-low-level-driver/42606
2025-12-09 1:48 AM
Hello
Just to summarize, but to be sure all of us have the information, Samsung provides fix for mobiles, i have updated my S24 with update, works fine now without App changes.
BR,FB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.