2022-10-20 4:48 AM
Hi,
I've got a x-nucleo board marked shield-m24sr-adv and I'm unable to find any docs about it. Well of course its a NFC reader board but.......
Solved! Go to Solution.
2022-10-20 5:53 AM
Welcome, @LePluc, to the community!
Unfortunately, there is officially no more information about the SHIELD-M24SR-ADV, since it only existed for a short time. It was then replaced by the very similar successor X-NUCLEO-NFC01A1, which is based on the same NFC chip M24SR64-YMN6T/2.
Regards
/Peter
2022-10-20 5:53 AM
Welcome, @LePluc, to the community!
Unfortunately, there is officially no more information about the SHIELD-M24SR-ADV, since it only existed for a short time. It was then replaced by the very similar successor X-NUCLEO-NFC01A1, which is based on the same NFC chip M24SR64-YMN6T/2.
Regards
/Peter
2022-10-20 5:56 AM
Hi,
I think this is rather a tag board than a reader board which seems to have been discontinued quite some years ago.
From a quick glimpse it seems very similar to x-nucleo-nfc01a1 which I would use instead because for it you find all kinds of support material.
Best Regards, Ulysses
2022-10-20 6:13 AM
Thanks for the swift answer!
2022-10-20 6:15 AM
Thanks for the swift answer, obsolete...well I guess that's what you get when store stuff in the wrong box :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.