2016-07-05 3:28 AM
Hello,
I've read product descriptions and FAQs, but still not clear about whether certain products offer me what I need.I'm interested in a product that consists of an MCU and an antenna, which allows me to read and write RFID messages. as a tagThe typical usecase is:1. the antenna alerts me of an incomming message2. I send a response. the response is sent exactly as I ordered - no self-added CRC or the likes.A big plus would be that the identification process is not done automatically, but I receive each message and respond to it myself.Can an ST product offer me this functionality? In which product?Thanks!Solved! Go to Solution.
2016-08-18 1:38 AM
Hello seeder.ilan,
The dynamic NFC memories are dual interface EEPROM, you need an MCU to communicate through i2c to access the EEPROM. 1. A product that is close to your application is the M24SR with GPO pin that can generate an interruption on the MCU (see for GPO feature) 2. With the M24SR you'll need to write the response in the EEPROM and then read it with a reader. Hope this help you. Kind Regards.2016-08-18 1:38 AM
Hello seeder.ilan,
The dynamic NFC memories are dual interface EEPROM, you need an MCU to communicate through i2c to access the EEPROM. 1. A product that is close to your application is the M24SR with GPO pin that can generate an interruption on the MCU (see for GPO feature) 2. With the M24SR you'll need to write the response in the EEPROM and then read it with a reader. Hope this help you. Kind Regards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.