2024-01-03 5:38 AM
Hello!
I am trying to read some blocks from a iso 15693 tag. I can do it with Android without any problem. But when I try to do it with iOS I always receive the response [255,255]. What does it mean?
For example:
22 33 E0 02 51 00 02 4E BE 55 08 00 32 00
Flags: 22
Function: 33 (Extended read multiple blocks)
Uid: E0 02 51 00 02 4E BE 55
Start block: 00 08
Number of blocks: 00 32
I don't know if the problem is the CRC16.
It occurs the same when I try to send the present password (B3 function), I receive the same response.
I know is not necessary to append it in Android, but, is it necessary in iOS?
which algorithm of CRC16 I have to use?
which bytes I have to use to generate CRC? all the message (22 33 E0 02 51 00 02 4E BE 55 08 00 32 00)?
Thank you!
Solved! Go to Solution.
2024-01-08 1:08 AM
Hi,
rather than diving straight into more elaborate commands I would start off with a standard read single block.
I would be surprised if the CRC would be needed by iOS. I think you you should be able to inspect STSW-ST25IOS002 which should show you how to use iOS for your use cases.
BR, Ulysses
2024-01-03 6:17 AM
Hi,
The UID is transmitted least significant byte first. In your trace "22 33 E0 02 51 00 02 4E BE 55 08 00 32 00 " the UID is most significant byte first.
Rgds
BT
2024-01-03 11:21 PM
Hi!
I tried:
22 33 55 BE 4E 02 00 51 02 E0 08 00 32 00
22 33 55 BE 4E 02 00 51 02 E0 08 00 32 00 0E 7F
22 33 55 BE 4E 02 00 51 02 E0 08 00 32 00 7F E0
And the same code appears [255,255]. ¿what does that code mean?
thank you in advance
2024-01-08 1:08 AM
Hi,
rather than diving straight into more elaborate commands I would start off with a standard read single block.
I would be surprised if the CRC would be needed by iOS. I think you you should be able to inspect STSW-ST25IOS002 which should show you how to use iOS for your use cases.
BR, Ulysses
2024-01-11 1:44 AM
Great! I did it and I can read all the memory. Now I will try to read multiple blocks.
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.