2021-10-15 3:12 AM
Hi there! I was wondering if I am able to obtain 3 axis data from LIS2DW12 using Steval-Smartag 1 board. If this is possible could you provide the software and programs to be installed.
Thanks!
Solved! Go to Solution.
2021-10-15 4:51 AM
Hi @JLiew.1162 ,
you can refer to the FP-SNS-SMARTAG1 function pack, that implements some examples with the Steval-Smartag 1 board and motion and environmental sensors.
In particular, you can refer to the below functions, that you can find in the \Drivers\BSP\SmarTag folder (SmarTag_motion_sensors.c):
int32_t SMARTAG_MOTION_SENSOR_GetAxesRaw(uint32_t Instance, uint32_t Function, SMARTAG_MOTION_SENSOR_AxesRaw_t *Axes)
int32_t SMARTAG_MOTION_SENSOR_GetAxes(uint32_t Instance, uint32_t Function, SMARTAG_MOTION_SENSOR_Axes_t *Axes)For the NFC transmission you probably have to call this other function in the main.c:
void MEMS_Sensors_ReadData(void)If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-10-15 4:51 AM
Hi @JLiew.1162 ,
you can refer to the FP-SNS-SMARTAG1 function pack, that implements some examples with the Steval-Smartag 1 board and motion and environmental sensors.
In particular, you can refer to the below functions, that you can find in the \Drivers\BSP\SmarTag folder (SmarTag_motion_sensors.c):
int32_t SMARTAG_MOTION_SENSOR_GetAxesRaw(uint32_t Instance, uint32_t Function, SMARTAG_MOTION_SENSOR_AxesRaw_t *Axes)
int32_t SMARTAG_MOTION_SENSOR_GetAxes(uint32_t Instance, uint32_t Function, SMARTAG_MOTION_SENSOR_Axes_t *Axes)For the NFC transmission you probably have to call this other function in the main.c:
void MEMS_Sensors_ReadData(void)If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-10-15 5:17 AM
Dear @Eleon BORLINI ,
Thanks for the quick reply! Sorry could you clarify if any software would be required to run this code? As I currently obtain measurements from the SMARTAG-1 by using a ST25R3911B-DISCO reader.
Thanks again,
Jia Xiang
2021-10-15 6:31 AM
Hi Jia,
you can use the STM32CubeIDE to build the project.
You can program it by connecting P201 is a JTAG/SWD interface to assist in software development. It can be connected to an external ST-LINK/V2 device using a 9-pin Cortex-M adapter.
-Eleon
2021-10-15 6:51 AM
Dear Eleon,
Thanks for the reply. To clarify, would I be able to build the project using STM32CubeIDE and program it with a ST25R3911B-DISCO reader wirelessly?
Thanks and have a great weekend,
Jia Xiang
2021-10-15 7:51 AM
Hi Jia,
I'm afraid that the ST25R3911B-DISCO is not capable of FOTA or similar, but you might update the firmware as shown in this video, using the dedicated ST25R3911B-DISCO GUI.
Have a nice weekend you too!
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.