2024-07-26 2:58 PM
I am porting the rfal and ndef for an ST25R3918 to zephyr. I have the rfal 3.0 working and i have ndef v1.0.4 i am getting errors for the ndef layer and was wondering if this is the correct ndef. I can read the UUID with RFAL so i know i can communicate with the tag. Below is the error. I do still have some timing errors to work out with the rtos and ISR servicing can be an issue.
appNFC: NDEF NOT DETECTED (ndefPollerNdefDetect returns 5)
Thanks,
Ed
Solved! Go to Solution.
2024-08-02 5:01 PM
So I did update the ndef lib to the one from 1.6sw release. After doing some digging I figured out that error was a need for more heap. After that I was able to get the nfc working. The example someone posted for zephyr had some issues that needed to be fixed.
2024-07-29 1:23 AM
Hi,
can you share more information about your setup:
ndef v1.0.4 is quite old. I would suggest to use a more recent one for example the latest one from the ST25 embedded NFC library. I believe this will not solve your issue but at least a recent NDEF middleware will be used.
To debug your issue, set a breakpoint in ndefTxTPollerNdefDetect where x=2, 3, 4 or 5 depending on the tag type being used (T2T, T3T, T4T or T5T). Then step until ERR_REQUEST is returned.
Rgds
BT
2024-08-02 5:01 PM
So I did update the ndef lib to the one from 1.6sw release. After doing some digging I figured out that error was a need for more heap. After that I was able to get the nfc working. The example someone posted for zephyr had some issues that needed to be fixed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.