2019-09-27 3:43 AM
Hi,
I'm using ST25r3911 for my project and have to work on DESFire card. I know there is code support for ISO/IEC 14443 cards on STSW-ST25R002. We can use DESFire as T4T for read and write. Is there any example of how to perform read/write?
Also is there any support for Authentication on STSW SDK?
Solved! Go to Solution.
2019-10-01 1:16 AM
Hi,
for your information,
I personally would recommend to move to the latest version of the RFAL.
Rgds
BT
2019-09-30 6:57 AM
Hi,
rfal_t4t.c provides API to compose ISO 7816 APDU. Some examples of how to use these API can be found in X-CUBE-NFC5 package (file ndef_t4t.c).
Rgds
BT
2019-09-30 7:12 AM
Hi,
we don't have sample code showing how to do things like authentication. However the interface described by Brian allows you to send any APDUs to perform authentication.
Regards, Ulysses
2019-09-30 8:44 PM
Hi Brain/Ulysses,
Thanks a lot for your recommendations. Actually I have an old version of NFC5 package(ver 1.2) which apparently doesn't have ndef files.
So I started working on the code which was provided on that version in demo.c to send APDU for select app, select file and read binary.
I was able to communicate successfully with the tag for the select functions but somehow got stuck on read binary which I'm sorting out now.
Meanwhile I downloaded NFC5&NFC6 latest versions to check the functionalities.
When I compare the main function(ISO-DEP Blocking Transceive) to exchange APDU on these 2 versions and the older one which I have it's still the same. Which means nothing much have changed on the Tx/Rx part but yes there is lot of changes when it comes to how the apdu's are packaged and other variables.
Just want to confirm...Can I continue working on NFC5 version 1.2 for the other apdu's like read and write or should I get the latest NFC package version?
My only worry is that I need to port in lot of code changes from the new version and I'm kind of going low on memory.
Regard,
Sach
2019-10-01 1:16 AM
Hi,
for your information,
I personally would recommend to move to the latest version of the RFAL.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.