2015-11-22 10:24 PM
HI,
I wanted to interact with X-NUCLEO-NFC01A1 (m24sr NFC dynamic tag ) by interfacing it with embedded linux board. I have googled and found this link and code : https://github.com/whaleygeek/pi_m24sr Is there any other sample code and hardware interfacing (sda,scl,vdd etc) information for interfacing m24sr with embedded board and using it for reading.writing. Or any m24sr linux drivers? Kindly let me know soon ! Thanks and Rgds, Rp #nfc01a1 #linux-driver #m24srSolved! Go to Solution.
2015-11-23 6:47 AM
Hello,
Sample code for interacting with X-NUCLEO-NFC01A1 can be found on the page related to:Dynamic NFC tag expansion board based on M24SR for STM32 Nucleo
http://www.st.com/web/en/catalog/tools/PF260759
and specifically the Firmware for STM32F103 to communicate through the I2C interface to the M24SR device
http://www.st.com/web/en/catalog/tools/PF259178
Please be aware this example code is developed for ST32 ARM core, and not Linux.SDA and SCL are the standard I2C signals which are available on the Arduino connector CN1 header.
VDD and VSS must be supplied on the power and ground connections on CN2.
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00122547.pdf
offers more information on the X-NUCLEO-NFC01A1 board itselfWe hope it will help you.
Best regards, Have a good day2015-11-23 6:47 AM
Hello,
Sample code for interacting with X-NUCLEO-NFC01A1 can be found on the page related to:Dynamic NFC tag expansion board based on M24SR for STM32 Nucleo
http://www.st.com/web/en/catalog/tools/PF260759
and specifically the Firmware for STM32F103 to communicate through the I2C interface to the M24SR device
http://www.st.com/web/en/catalog/tools/PF259178
Please be aware this example code is developed for ST32 ARM core, and not Linux.SDA and SCL are the standard I2C signals which are available on the Arduino connector CN1 header.
VDD and VSS must be supplied on the power and ground connections on CN2.
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00122547.pdf
offers more information on the X-NUCLEO-NFC01A1 board itselfWe hope it will help you.
Best regards, Have a good day2015-11-23 8:30 PM
2015-11-27 4:49 AM
Hi,
At this time, we do not have sample code under Linux platform for m24sr. To communicate with the m24sr you can connect it through the I²C of your Linux board (for example, I've attached a picture of connection between Raspberry Pi and m24sr, with X-NUCLEO-NFC01A1). Then you can use the driver for m24sr from the STM32 software package and port it to the Linux environment. Hope this will help you. Kind Regards ________________ Attachments : Pi_M24SR.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzLL&d=%2Fa%2F0X0000000bKT%2FfAbKhL_AdVJ44KBfIOV4B5l6My3U10rcuEaDpxaINnY&asPdf=false2015-11-29 7:56 PM
2015-11-30 8:32 AM
Hello,
Figure 17, page 71 of the M24SR datasheethttp://www.st.com/web/en/resource/technical/document/datasheet/DM00067892.pdf
will give you maximum values of the resistance to use on the SCL/SDA signals. We hope this will help you. Have a good day.2015-12-08 4:28 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.