2024-10-25 3:52 AM
Hello STM Community,
I'm currently working on a project involving the ST25DV04KC-IE8C3 NFC chip interfaced with the STM32L496ZG microcontroller. I've encountered an issue where the performance of the NFC chip deteriorates when a magnet is brought near the system, specifically related to the operation of a magnetic switch that generates interrupts.
I have attached a photo of the PCB layout for your reference. I would greatly appreciate any feedback on the design or suggestions on mitigating this issue!
Thank you for your assistance!
Solved! Go to Solution.
2024-10-25 7:10 AM
Hello,
NFC is based on magnetic coupling between the reader and the tag. The reader is emitting a magnetic field at 13.56MHz that is captured by the tag's antenna, creating current into the antenna. Having a magnet nearby may disturb the magnetic field emitted by the reader.
Does the issue appear when there is a reader communicating with the tag and a magnet is put close to the switch? Or do you have issues when there is no RF reader in front of the tag?
Best regards.
2024-10-25 7:10 AM
Hello,
NFC is based on magnetic coupling between the reader and the tag. The reader is emitting a magnetic field at 13.56MHz that is captured by the tag's antenna, creating current into the antenna. Having a magnet nearby may disturb the magnetic field emitted by the reader.
Does the issue appear when there is a reader communicating with the tag and a magnet is put close to the switch? Or do you have issues when there is no RF reader in front of the tag?
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.