2025-03-25 2:11 AM
Hi
I Reported this for Improvement in STSW-ST25RFAL 3.0 source before.
Now STSW-ST25RFAL 4.0 is available but the following problems are not changed.
1) Add to rfal_analogConfig.h, rfal_crc.h, rfal_iso15693_2.h header files.
#if defined( __cplusplus )
extern "C" {
#endif
otherwise this file makes it difficult with C++
2) Add to rfal_analogConfig.h header files.
#if !defined( __cplusplus )
typedef struct {
uint8_t id[sizeof(rfalAnalogConfigId)];
rfalAnalogConfigNum num;
rfalAnalogConfigRegAddrMaskVal regSet[];
} rfalAnalogConfig;
#else
struct rfalAnalogConfig;
#endif
C++ can't handle an empty array regSet[] in a struct
Solved! Go to Solution.
2025-03-27 3:21 AM
Hi,
ad 1)
I better understand now the point of it being more convenient in a mixed C/C++ environment. If implementing such we would need to also enforce this for all our files/test it. We will keep it on our consideration list but spreading a few <"extern "C" {}> in C++ I don't consider blocking.
ad 2)
This will likely require using one of the flexible array workarounds - putting a 0 or 1 into the square brackets for rfalAnalogConfigRegAddrMaskVal regSet[] - also ANYSIZE_ARRAY (MS discussion) might be used - offloading to rfal_platform. Again here we will consider but don't expect soon an action.
Sorry, Ulysses
2025-03-25 4:59 AM
Hi CanRF,
actually we have not concluded that it really is a good idea to spread these macros. IMO they don't hinder you from using the sources as you could
extern "C" {
#include "rfal_rf.h"
}Spreading the proposed #defined(__cplusplus) would prevent the first use case.
BR, Ulysses
2025-03-26 7:24 AM
Hi
1)
Every serious library owner adds this to every header file.
See STCube, CMSIS, C-Library, ...
So please add this too
2)
The problem with empty array in a struct is not solved with
extern "C" {
#include "rfal_analogConfig.h"
}
2025-03-26 7:46 AM - edited 2025-03-26 8:21 AM
Hi,
just because some people do it this way does not necessarily mean they are right.
I tend to agree to e.g. this discussion here:
https://github.com/micropython/micropython/issues/3488
with more meat:
https://www.microforum.cc/blogs/entry/34-using-extern-c/
https://arne-mertz.de/2018/10/calling-cpp-code-from-c-with-extern-c/
Please explain your second point.
BR, Ulysses
2025-03-26 8:55 AM
Hi,
1)
From
https://github.com/micropython/micropython/issues/3488
OTOH, having these wrappers in C headers is very common and does make C++ integration easier. It requires updating not only py/.h files but also lib/.h and extmod/*.h. We can do this if there's enough interest from the community.
So You update the Header once. Otherwise ever C++ project do it again.
From
https://www.microforum.cc/blogs/entry/34-using-extern-c/
Is a discussion about PIC16 code where a C++ compiler is not available and so extern "C" not necessary.
But for STM32 a C++ Compiler is available and used from us and other developer.
It is not useful to compile all source file as C++. They are not tested as C++.
So C File should compile as C and CPP File should compile as C++.
But on the Interface the C++ Compiler should not add name-mangling.
So it would be helpful when ST Code has got always the same coding style.
2)
typedef struct {
uint8_t id[sizeof(rfalAnalogConfigId)];
rfalAnalogConfigNum num;
rfalAnalogConfigRegAddrMaskVal regSet[];
} rfalAnalogConfig;
Results with C++ in an error because C++ does not support empty array[] at the end of a struct.
GC++ does support this but not ANSI C++.
Inside the header only the pointer to rfalAnalogConfig is used.
So C/C++ supports a forward deceleration with
struct rfalAnalogConfig;
But the C Module also need the details about the struct.
So my solution is to define a forward declaration for C++ use (extern) and a C compatible declaration for C use.
2025-03-27 3:21 AM
Hi,
ad 1)
I better understand now the point of it being more convenient in a mixed C/C++ environment. If implementing such we would need to also enforce this for all our files/test it. We will keep it on our consideration list but spreading a few <"extern "C" {}> in C++ I don't consider blocking.
ad 2)
This will likely require using one of the flexible array workarounds - putting a 0 or 1 into the square brackets for rfalAnalogConfigRegAddrMaskVal regSet[] - also ANYSIZE_ARRAY (MS discussion) might be used - offloading to rfal_platform. Again here we will consider but don't expect soon an action.
Sorry, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.