2023-05-26 6:53 PM
Solved! Go to Solution.
2023-05-29 1:15 AM
Hi,
ST25R3911B-DISCO is a ready-to-use kit with a PC GUI interacting with the embedded FW. The source code for the FW is available in STSW-ST25R002 (Firmware for ST25R3911B-DISCO kit (Source)) with a Keil µVision project. The support of STM32Cube is not provided.
If you are looking for a development board with FW package available for STM32Cube, I would rather recommand to use the X-NUCLEO-NFC05A1 board and the X-CUBE-NFC5 FW package.
Rgds
BT
2023-05-29 12:45 AM
Hi
which NFC module are you referring to? NFC dynamic tag or NFC reader?
A Firmware package is avalable for each NFC expansion board on st.com. For example, for the X-NUCLEO-NFC08A1 reader board, a X-CUBE-NFC6 firmware package is avalable and it contains some demo projects for STM32CubeIDE.
Rgds
BT
2023-05-29 1:06 AM
I am using the ST25R3911B-DISCO board, which is an NFC reader. Which NFC firmware package does this board use?
2023-05-29 1:15 AM
Hi,
ST25R3911B-DISCO is a ready-to-use kit with a PC GUI interacting with the embedded FW. The source code for the FW is available in STSW-ST25R002 (Firmware for ST25R3911B-DISCO kit (Source)) with a Keil µVision project. The support of STM32Cube is not provided.
If you are looking for a development board with FW package available for STM32Cube, I would rather recommand to use the X-NUCLEO-NFC05A1 board and the X-CUBE-NFC5 FW package.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.