2019-05-28 12:16 AM
Hello Sir
Is CR95HF support sony FeliCa function? if yes, any software library or samples available for reference? if Not, which part can support Felica?
Thank you.
Solved! Go to Solution.
2019-05-29 12:57 AM
Hi,
the following readers of the ST25R family provide NFC-F / FeliCa™ reader mode support:
Note: for new developments, ST recommends to use ST25R95 in replacement of CR95HF/ST95HF (see your local ST representative for further information).
ST25R95 is the convergence device for CR95HF and ST95HF.
A demo of ST25R95/CR95HF/ST95HF reader features (polling tags for various technologies including NFC-F and displaying UID) is included in the X-CUBE-NFC3 v2.0.0 package. This package provides an RF Abstraction Layer common with other readers of the ST25R family.
This software package is ready to run on X-NUCLEO-NFC03A1 expansion board with either NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB STM32 boards.
Rgds
BT
2019-05-29 12:57 AM
Hi,
the following readers of the ST25R family provide NFC-F / FeliCa™ reader mode support:
Note: for new developments, ST recommends to use ST25R95 in replacement of CR95HF/ST95HF (see your local ST representative for further information).
ST25R95 is the convergence device for CR95HF and ST95HF.
A demo of ST25R95/CR95HF/ST95HF reader features (polling tags for various technologies including NFC-F and displaying UID) is included in the X-CUBE-NFC3 v2.0.0 package. This package provides an RF Abstraction Layer common with other readers of the ST25R family.
This software package is ready to run on X-NUCLEO-NFC03A1 expansion board with either NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB STM32 boards.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.