2020-10-21 12:20 AM
Dear Sirs
I have run PollingTagDetect application project on NUCLEO-L053R8 + X-NUCLEO-NFC05A1 board successfully. And I have transferred PollingTagDetect project code to NUCLEO-G070RB + X-NUCLEO-NFC05A1 platform. The terminal software can display ISO15693 UID and block data. But while scan ISO14443A tag the HardFault occurred immediately.
Do you know the root cause? Are both Middlewares and ST25R3911B driver able to run on STM32G070R8 CPU?
Thanks,
Phil Huang
Solved! Go to Solution.
2020-10-21 1:20 AM
Hi Phil,
from top level it seems very much like the issue in this thread:
Please check if similar restrictions exist in STM32G0 SPI driver code.
Regards, Ulysses
2020-10-21 1:20 AM
Hi Phil,
from top level it seems very much like the issue in this thread:
Please check if similar restrictions exist in STM32G0 SPI driver code.
Regards, Ulysses
2020-10-21 7:11 PM
Hi Ulysses
It works. Thank you.
Regards,
Phil
2020-10-21 11:41 PM
Hi Phil,
could you share a few more details please? Did my answer help? Was it the same issue?
I think other people in the community would appreciate.
Regards, Ulysses
2020-10-22 1:09 AM
Hi Ulysses
Following your suggestion I modified the spi HAL driver stm32g0xx_hal_spi.c file. Bucause access ST25R3911B register via HAL_SPI_TransmitReceive function only so I modified line 1329 and 1399 code.
The original code is
*((uint16_t *)hspi->pRxBuffPtr) = (uint16_t)hspi->Instance->DR;
After modified code is
//*((uint16_t *)hspi->pRxBuffPtr) = (uint16_t)hspi->Instance->DR;
uint16_t temp;
temp = (uint16_t)hspi->Instance->DR;
*((uint8_t *)hspi->pRxBuffPtr) = temp & 0xff;
*(((uint8_t *)hspi->pRxBuffPtr)+1) = temp >> 8;
After download new image, reader do not occur HardFault_IRQ while scan ISO14443A tag. And can display ISO14443A UID on PC terminal software.
Best regards,
Phil Huang
2020-10-22 8:06 AM
Hi Phil,
thanks for sharing!
Best Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.