2020-02-22 2:02 PM
en.x-cube-nfc3
Nucleo SMTM32F103RB Project
How to send the messages also thru an additional UART port (the same comments which are sent by the Nucleo USB port also sent by an additional UART of the Nucleo board)
Thanks
Is the CubeMX Project available for the en.x-cube-nfc3 projects?
Solved! Go to Solution.
2020-02-24 2:26 AM
Hi,
here is a ioc file for STM32CubeMx.
Just for my curiosity, why do you need to duplicate the traces on an additional port?
Basically, you need to:
Rgds
BT
2020-02-24 2:26 AM
Hi,
here is a ioc file for STM32CubeMx.
Just for my curiosity, why do you need to duplicate the traces on an additional port?
Basically, you need to:
Rgds
BT
2020-02-24 9:11 AM
Dear Brian.
Thanks for your answer.
I needed this for getting the EVBs (STM32F103RB Nucleo + X-NUCLEO-NFC03A1) working ASAP.
I needed to connect the EVBs to my equipment thru a RS-232.
Reading the Nucleo user manual, I saw that the UART at CN3 was available for this. I used it and it worked.
Now, I only need to remove the logger mesagges and keep the ID data for passing it to my equipment. With this,
Thus, I can build a demo for demonstrating that the system works.
Then, the software engineers will optimize the code meanwhile I will design a board with the CR95HF and the SMT32F103RB.
Anyway, I'll try to use the .ioc you have sent. Also, I'll use it for trying to port the project to the STM32F103C6. This will allow us to design a cheaper board.
Thanks again.
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.