cancel
Showing results for 
Search instead for 
Did you mean: 

Does ST25R3920B support MIFARE ?

zhangxixun
Associate III

I am now using your company's ST25R3920B as a digital key reader.

I would like to ask, does the SDK of 3920B support the Philips communication protocol of MIFARE Classic cards?

If so, where can I see it?

THANKS

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

see details in https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/nfc0541-read-mifare-classic-1k/m-p/255197 and other posts related to mifare on this community. 

Also, some devices based on ST25R391x, such as the Flipper Zero, supports Mifare tags. Refer to the Flipper Zero firmware source code for more details.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Brian TIDAL
ST Employee

Hi,

see https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/if-the-st25r3916-is-compatible-with-nxp-s-tag-reader/td-p/384917 for similar question.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
zhangxixun
Associate III

Hi Brian

thanks for you reply.

how can I set the "Low level modes " in 3920B?

Hi,

see details in https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/nfc0541-read-mifare-classic-1k/m-p/255197 and other posts related to mifare on this community. 

Also, some devices based on ST25R391x, such as the Flipper Zero, supports Mifare tags. Refer to the Flipper Zero firmware source code for more details.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
zhangxixun
Associate III

Hi Brian

thanks for your kindly reply.

zhangxixun
Associate III

Hi Brian

 I would like to ask, where can I find the API function interface for reading and writing mifare cards?

Or, which API interface functions should I call to realize data interaction between 3920B and M1 card? Are there any application notes for reference?

Hi,

Such tags use proprietary commands and proprietary authentication/ciphering. As explained in the various posts, the ST25R3920 provides support for the specific framing used by such tags but implementation for the proprietary commands/authentication/ciphering is not provided in the ST25R reference firmware. See the various links in the previous posts for more details.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.