cancel
Showing results for 
Search instead for 
Did you mean: 

cr95hf not detecting nfc tag (ISO/IEC 14443-A) with ardunio

Rsana.1
Associate II

hi,

I have connected cr95hf with ardunio uno, I am able to receive the response for IDN command correctly ,and set the protocol (ISO/IEC 14443-A) ,but the tag is not detecting, I have attached the code and response logs. I would like to know whats wrong with my code .I have taken the reference code code from the following link

https://community.st.com/s/global-search/cr95hf%20esp8266

I have have changed only protocol,and done the wiring as mentioned in the code

response in serial monitor:

Started

IDN COMMAND-

RESPONSE CODE: 0 LENGTH: 15

DEVICE ID: 4E 46 43 20 46 53 32 4A 41 53 54 34 0  

ROM CRC: 2ACE 

PROTOCOL SET-

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 87

some times Iam getting response as below,

#include <SPI.h>
 
const int SSPin = 10;  // Slave Select pin
const int IRQPin = 2;  // Sends wake-up pulse
byte TXBuffer[40];     // transmit buffer
byte RXBuffer[40];     // receive buffer
byte NFCReady = 0;     // used to track NFC state
 
 
void setup() {
    pinMode(IRQPin, OUTPUT);
    digitalWrite(IRQPin, HIGH); // Wake up pulse
    pinMode(SSPin, OUTPUT);
    digitalWrite(SSPin, HIGH);
 
    Serial.begin(9600);
    Serial.println("Started");
    SPI.begin();
    SPI.setDataMode(SPI_MODE0);
    SPI.setBitOrder(MSBFIRST);
    SPI.setClockDivider(SPI_CLOCK_DIV32);
 
 // The CR95HF requires a wakeup pulse on its IRQ_IN pin
 // before it will select UART or SPI mode.  The IRQ_IN pin
 // is also the UART RX pin for DIN on the BM019 board.
 
    delay(10);                      // send a wake up
    digitalWrite(IRQPin, LOW);      // pulse to put the 
    delayMicroseconds(100);         // BM019 into SPI
    digitalWrite(IRQPin, HIGH);     // mode 
    delay(10);
}
 
 
 
 
void IDN_Command()
 {
 byte i = 0;
 
// step 1 send the command
  digitalWrite(SSPin, LOW);
  SPI.transfer(0);  // SPI control byte to send command to CR95HF
  SPI.transfer(1);  // IDN command
  SPI.transfer(0);  // length of data that follows is 0
  digitalWrite(SSPin, HIGH);
  delay(1);
 
// step 2, poll for data ready
// data is ready when a read byte
// has bit 3 set (ex:  B'0000 1000')
 
  digitalWrite(SSPin, LOW);
  while(RXBuffer[0] != 8)
    {
    RXBuffer[0] = SPI.transfer(0x03);  // Write 3 until
    RXBuffer[0] = RXBuffer[0] & 0x08;  // bit 3 is set
    }
  digitalWrite(SSPin, HIGH);
  delay(1);
 
 
// step 3, read the data
  digitalWrite(SSPin, LOW);
  SPI.transfer(0x02);   // SPI control byte for read         
  RXBuffer[0] = SPI.transfer(0);  // response code
  RXBuffer[1] = SPI.transfer(0);  // length of data
  for (i=0;i<RXBuffer[1];i++)      
      RXBuffer[i+2]=SPI.transfer(0);  // data
  digitalWrite(SSPin, HIGH);
  delay(1);
 
  if ((RXBuffer[0] == 0) & (RXBuffer[1] == 15))
  {  
    Serial.println("IDN COMMAND-");  //
    Serial.print("RESPONSE CODE: ");
    Serial.print(RXBuffer[0]);
    Serial.print(" LENGTH: ");
    Serial.println(RXBuffer[1]);
    Serial.print("DEVICE ID: ");
    for(i=2;i<(RXBuffer[1]);i++)
    {
      Serial.print(RXBuffer[i],HEX);
      Serial.print(" ");
    }
    Serial.println(" ");
    Serial.print("ROM CRC: ");
    Serial.print(RXBuffer[RXBuffer[1]],HEX);
    Serial.print(RXBuffer[RXBuffer[1]+1],HEX);
    Serial.println(" ");
  }
  else
    Serial.println("BAD RESPONSE TO IDN COMMAND!");
 
  Serial.println(" ");
}
 
 
 
 
void SetProtocol_Command()
 {
 byte i = 0;
 
// step 1 send the command
  digitalWrite(SSPin, LOW);
  SPI.transfer(0x00);  // SPI control byte to send command to CR95HF
  SPI.transfer(0x02);  // Set protocol command
  SPI.transfer(0x02);  // length of data to follow
  SPI.transfer(0x02);  // code for ISO/IEC 14443-A
  SPI.transfer(0x00);  // Wait for SOF, 10% modulation, append CRC
  digitalWrite(SSPin, HIGH);
  delay(1);
 
// step 2, poll for data ready
 
  digitalWrite(SSPin, LOW);
  while(RXBuffer[0] != 8)
    {
    RXBuffer[0] = SPI.transfer(0x03);  // Write 3 until
    RXBuffer[0] = RXBuffer[0] & 0x08;  // bit 3 is set
    }
  digitalWrite(SSPin, HIGH);
  delay(1);
 
// step 3, read the data
  digitalWrite(SSPin, LOW);
  SPI.transfer(0x02);   // SPI control byte for read         
  RXBuffer[0] = SPI.transfer(0);  // response code
  RXBuffer[1] = SPI.transfer(0);  // length of data
  digitalWrite(SSPin, HIGH);
 
  if ((RXBuffer[0] == 0) & (RXBuffer[1] == 0))
  {
     Serial.println("PROTOCOL SET-");  //
     NFCReady = 1; // NFC is ready
  }
  else
  {
     Serial.println("BAD RESPONSE TO SET PROTOCOL");
     NFCReady = 0; // NFC not ready
  }
  Serial.println(" ");
}
 
 
 
void Inventory_Command()
 {
 byte i = 0;
 
// step 1 send the command
  digitalWrite(SSPin, LOW);
  SPI.transfer(0x00);  // SPI control byte to send command to CR95HF
  SPI.transfer(0x04);  // Send Receive CR95HF command
  SPI.transfer(0x03);  // length of data that follows is 0
  SPI.transfer(0x26);  // request Flags byte
  SPI.transfer(0x02);  // Inventory Command for ISO/IEC 14443-A
  SPI.transfer(0x00);  // mask length for inventory command
  digitalWrite(SSPin, HIGH);
  delay(1);
 
// step 2, poll for data ready
// data is ready when a read byte
// has bit 3 set (ex:  B'0000 1000')
 
  digitalWrite(SSPin, LOW);
  while(RXBuffer[0] != 8)
    {
    RXBuffer[0] = SPI.transfer(0x03);  // Write 3 until
    RXBuffer[0] = RXBuffer[0] & 0x08;  // bit 3 is set
    }
  digitalWrite(SSPin, HIGH);
  delay(1);
 
 
// step 3, read the data
  digitalWrite(SSPin, LOW);
  SPI.transfer(0x02);   // SPI control byte for read
  RXBuffer[0] = SPI.transfer(0);  // response code
  RXBuffer[1] = SPI.transfer(0);  // length of data
  for (i=0;i<RXBuffer[1];i++)
      RXBuffer[i+2]=SPI.transfer(0);  // data
  digitalWrite(SSPin, HIGH);
  delay(1);
 
  if (RXBuffer[0] == 128)
  {  
    Serial.println("TAG DETECTED");
    Serial.print("UID: ");
 
    for(i=11;i>=4;i--)
    {
      Serial.print(RXBuffer[i],HEX);
      Serial.print(" ");
    }
    Serial.println(" ");
        delay(500);
  }
  else
    {
    Serial.print("NO TAG IN RANGE - ");
    Serial.print("RESPONSE CODE: ");
    Serial.println(RXBuffer[0],HEX);
    }
  Serial.println(" ");
}
 
 
void loop() {
  if(NFCReady == 0)
  {
    IDN_Command();  // reads the CR95HF ID
    delay(1000);
    SetProtocol_Command(); // ISO 14443-A settings
    delay(1000);
  }
  else
  {
    Inventory_Command();
    delay(1000);
  }
}

Started

IDN COMMAND-

RESPONSE CODE: 0 LENGTH: 15

DEVICE ID: 4E 46 43 20 46 53 32 4A 41 53 54 34 0  

ROM CRC: 2ACE 

BAD RESPONSE TO SET PROTOCOL

Started

Started

Started

BAD RESPONSE TO IDN COMMAND!

BAD RESPONSE TO SET PROTOCOL

Started

Started

Started

Started

Started

Started

Started

Started

Started

BAD RESPONSE TO IDN COMMAND!

BAD RESPONSE TO SET PROTOCOL

BAD RESPONSE TO IDN COMMAND!

BAD RESPONSE TO SET PROTOCOL

BAD RESPONSE TO IDN COMMAND!

PROTOCOL SET-

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 1C

NO TAG IN RANGE - RESPONSE CODE: 87

NO TAG IN RANGE - RESPONSE CODE: 0

NO TAG IN RANGE - RESPONSE CODE: 18

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi

REQA/WUPA are part of the ISO14443-3 command set.

A complete polling loop example is provided in X-CUBE-NFC3. This includes the NFC-A/ISO14443-A technology detection and anti-collision.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Brian TIDAL
ST Employee

Hi,

can you describe your HW enviroment e.g. X-NUCLEO-NFC03A1 board connected to Arduino or BM019 board connected to Arduino?

Inventory command is an ISO15693-3 command. ISO14443-A tags do not reply to Inventoty command but to REQA or WUPA commands.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi,

I have a custom board in which we have CR95HF Ic is interfaced with esp32d2wd ic, but I have soldered jumper wires for spi lines (miso mosi,ss,clk) and IRQ_IN, and connected to ardunio board I am able to receive the response to IDN command it means my wiring is correct and spi communication is working fine.can you provide any example code for detecting ISO14443-A tags , as you said that ISO14443-A tags do not reply to Inventoty command but to REQA or WUPA commands,what is REQA or WUPA commands ,can you provide any code with these commands

Brian TIDAL
ST Employee

Hi

REQA/WUPA are part of the ISO14443-3 command set.

A complete polling loop example is provided in X-CUBE-NFC3. This includes the NFC-A/ISO14443-A technology detection and anti-collision.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.