2023-09-20 2:14 AM
Is it possible to transfer large data files, meaning bigger than the internal memory of the tag?
The intended purpose is to have a stm32 connected to an i²c dynamic tag and be able to write large files, like a new firmware, to the stm32 MCU. The problem is, that I couldn't find documentation if it is possible to simultaneously read the data via i²c which is currently written to the tag via NFC. If not possible in a continues stream, reading in chunks would be a viable alternative. As long as it is possible to do in one NFC "Session". That would allow a 0 port device that can be sealed towards the environment.
Solved! Go to Solution.
2023-09-20 5:12 AM
For example, you could look at the software package STSW-ST25DV001, which deals with this topic.
Good luck!
/Peter
2023-09-20 5:12 AM
For example, you could look at the software package STSW-ST25DV001, which deals with this topic.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.