2020-11-19 7:32 AM
Hi, I have a custom board with the st25r95 . I have changed the platfrom.h file and I am able to read UUID, but I need the device to be in card emulation mode if i set RFAL_FEATURE_LISTEN_MODE to true
I am getting a linker error:
In file rfal_rfst25r95.c
undefined reference to `st25r95Listen'
undefined reference to `st25r95RearmListen'
undefined reference to `st25r95SetACFilter'
undefined reference to `st25r95SPIGetLmState'
And it seems that this functions are not implemented!
Is there any working example, or documentation to implement card emulation?
Solved! Go to Solution.
2020-11-19 8:12 AM
Hi,
thanks for using ST25R95/CR95HF product. Card Emulation source code is not part of the X-CUBE-NFC3 v2.1.0 but I will provide it to you in private.
Feel free to share more details about your card emulation application to help us to provide appropriate support.
Thanks
Rgds
BT
2020-11-19 8:12 AM
Hi,
thanks for using ST25R95/CR95HF product. Card Emulation source code is not part of the X-CUBE-NFC3 v2.1.0 but I will provide it to you in private.
Feel free to share more details about your card emulation application to help us to provide appropriate support.
Thanks
Rgds
BT
2021-12-15 11:36 PM
I also met the same problem, could you also send me the card emulation mode St25r95 demo, this is my email A15211163466@gmail.com
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SPIGetLmState (referred from st25r95_com_spi.o).
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95Listen (referred from rfal_rfst25r95.o).
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95PollField (referred from rfal_rfst25r95.o).
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95RearmListen (referred from rfal_rfst25r95.o).
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SPIGetLmState (referred from rfal_rfst25r95.o).
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SPISetACState (referred from rfal_rfst25r95.o).
STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SetACFilter (referred from rfal_rfst25r95.o).
2022-10-09 3:17 AM
Hello Sir
I met the same issue of build error with this chat, could you send the patch file to me? my email is d.shih@alfasemi.com.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.