2020-10-16 1:46 AM
Hello,
I use the ST25RU3993-EVAL board software.
I want to do some Tag settings.
Can I use the Generic Command (Tag Settings) to send Commands from the EPC Class 1Gen2 Standard?
it is possible, is their any explanation how to enter the Command?
Solved! Go to Solution.
2020-10-19 5:46 AM
Hi,
yes, you can use the Generic command to send any command defined in Gen2 and also proprietary command following the Gen 2 physical interface definition.
The Generic Command input mask has the following members
By default the "Generic Command" section in the "Tag Settings" dialog has pre-configured a Gen2 Read command, reading the first word in TID memory from address 0. (see EPCglobal Gen2 Read command specification)
Cmd Read (8bit) | MemBank (2bit) | WordPtr (EBV=8bit here) | WordCount (8bit) | RN (8bit) | CRC (8bit)
11000010 | 10 | 00000000 | 00000001 | AUTO when tick "Append RN16" | AUTO when use Direct Command 0x90
= > 0xC2 80 00 40, Tx valid bits = 26
In the example for the TAG reply of the Read command you need then to decode according to the Gen 2 spec
Header (1bit) | Memory Word (16bit) | RN (16bit)
=> 33bits expected, CRC is handled automatically when using Direct Command 0x90
2020-10-19 5:46 AM
Hi,
yes, you can use the Generic command to send any command defined in Gen2 and also proprietary command following the Gen 2 physical interface definition.
The Generic Command input mask has the following members
By default the "Generic Command" section in the "Tag Settings" dialog has pre-configured a Gen2 Read command, reading the first word in TID memory from address 0. (see EPCglobal Gen2 Read command specification)
Cmd Read (8bit) | MemBank (2bit) | WordPtr (EBV=8bit here) | WordCount (8bit) | RN (8bit) | CRC (8bit)
11000010 | 10 | 00000000 | 00000001 | AUTO when tick "Append RN16" | AUTO when use Direct Command 0x90
= > 0xC2 80 00 40, Tx valid bits = 26
In the example for the TAG reply of the Read command you need then to decode according to the Gen 2 spec
Header (1bit) | Memory Word (16bit) | RN (16bit)
=> 33bits expected, CRC is handled automatically when using Direct Command 0x90
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.