cancel
Showing results for 
Search instead for 
Did you mean: 

What exactly is the VCONN pin?

LauraCx
ST Employee

What exactly is the VCONN pin?

A USB Type-C™ connector has two Configuration Channel pins (CC1 and CC2) used for PDO (Power profile) negotiation.
Only one of these two pins is active during the communication; the other one can be used to power a small device or an active cable (for >3A). In this case, this pin is referred to as VCONN. VCONN is required only for source devices, not for sink.
 
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.

Version history
Last update:
‎2022-07-18 8:08 AM
Updated by: