cancel
Showing results for 
Search instead for 
Did you mean: 

The difference between STTH20003TV1 and STTH20003TV

robertw1
Associate II

Hello Team,

I found both STTH20003TV1 and STTH20003TV are available on the market.

Unfortunately, I cannot find STTH20003TV1 in ST datasheet.

STTH20003 - 300 V, 200 A Ultrafast Diode - STMicroelectronics

Could you provide the difference between STTH20003TV1 and STTH20003TV?

What's the meaning of suffix '1' in the part number?

Many thanks!

Robert

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

It is probably a little confusing, but the full order designation is actually STTH20003TV1, i.e. with the suffix 1. When the first devices were launched at the end of the last millennium, it was still marked 20003TV, which can still be found in many cases today, but in future this will probably be changed to 20003TV1.

However, this suffix 1 does not change the technical parameters of this dual rectifier, so it is purely a question of marking.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

It is probably a little confusing, but the full order designation is actually STTH20003TV1, i.e. with the suffix 1. When the first devices were launched at the end of the last millennium, it was still marked 20003TV, which can still be found in many cases today, but in future this will probably be changed to 20003TV1.

However, this suffix 1 does not change the technical parameters of this dual rectifier, so it is purely a question of marking.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
robertw1
Associate II

Hi Peter,

YES! Thank you for your reply!

Have a nice day!

Robert

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.