2023-12-21 10:59 PM
Hi Team.
I'm trying to connect STEVAL-GMBL02V1 board with STSW-GMBL02V1 control application.
The cursor icon becomes a standby animation, but I cannot connect.
I connected using the following steps:
Condition:
The thing to be concerned about is that when you connect USB, the current value decreases.
I am using a power supply that can only display up to two decimal places, but 40mA is displayed as 0A.
I would like to know if the board is defective or if there is a problem with the procedure.
Has anyone experienced a similar problem?
Solved! Go to Solution.
2024-02-12 2:33 AM
Hi Kenji and ST Team,
We also have the same problem we also cannot connect to the provided GUI.
Did you find a solution to this?
We followed the instructions:
- Flashed the Board with the provided executable from the website download and when we power the board by USB we get the flashing LED
- Installed the STM32 virtual COM Port Driver (our OS is Windows 11)
The device enumerates in device manager but we cannot connect to the APP GUI.
Best Regards,
Ross
2024-02-12 2:33 AM
Hi Kenji and ST Team,
We also have the same problem we also cannot connect to the provided GUI.
Did you find a solution to this?
We followed the instructions:
- Flashed the Board with the provided executable from the website download and when we power the board by USB we get the flashing LED
- Installed the STM32 virtual COM Port Driver (our OS is Windows 11)
The device enumerates in device manager but we cannot connect to the APP GUI.
Best Regards,
Ross
2024-02-12 3:00 AM
Hi all,
For reference this is now working and was solved by installing Windows 10 on a virtual machine and following the instructions again. Seems that there is some issue with Windows 11 and perhaps the Virtual COM Port driver.
Best Regards,
Ross
2024-02-12 6:28 PM
Hi RLW.
After rewriting the firmware, I was able to connect several times.
Also waiting a while after turning on the power, I was able to connect several times.
However, the connection remains unstable. Sometimes I can connect and sometimes I can't.
Even if I can connect, the application freeze.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.