2024-11-11 3:50 AM
Hi,
Working on a project involving the STSPIN840 motor driver connected to a PIC32MK microcontroller,trying to implement current sensing for accurate motor control. The STSPIN840 has the current sensing pins SNSA, SENSEA1, and SENSEA2 for each channel.
I would appreciate any advice on the following points:
Current Sensing Setup: What is the recommended configuration for using these pins to measure the motor current accurately?
RSNS = 330 mohm
Connection to ADC: connected the sense pins to the ADC of the PIC32MK. When reading ADC getting current values very high(in 10s of A ) compared to the the motor rated values(<1A)
Are there any particular considerations or issues I should be aware of when interfacing these pins with the microcontroller’s ADC?
Any insights, diagrams, or documentation references would be greatly appreciated!
Thank you in advance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.