2017-08-16 10:06 PM
We have purchased 10 qty of STL160NS3LLH7 MOSFET IC. We found that Drain to source impedance of MOSFETs is varying( NOTE : MOSFET were not connected to any external circuitry while measuring impedance using DMM). For some of the MOSFETs it was around 1kOhm for others it was 2kOhm and 3kOhm also. I am not getting same performance with all the MOSFETs. I think that this because of this variation in Drain to source impedance. I have never seen such a peculiar behavior of MOSFETs. Is it a manufacturing problem or these MOSFETs behave like this only? Please explain!
2017-08-31 6:29 AM
Hi,
Gate Source Voltage is fixed to 0 during these measurement?
this is import, otherwise if this value is different from zero, a small current could flow trough the MOSFET and could give different Drain to source impedance
regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.