2019-06-13 12:44 PM
Dear all,
we are evaluating STEVAL-IPFC01V1 board which is a PFC converter and we are experiences
problems when we change capacitor bank to larger value. At default board is equipped with
4x470uF, which we later changed to 4x1000uF plus 4x470uF. If we do that the third MOSFET in a row is blown up every time on power up. Using eDesign tool there is no limitation for this king of
capacitance and even eDesigner did calculate even larger capacitance.
I also generated firmware from eDesigner, but it looks like, that Udc link voltage is raised to
450V with selected 400V DC link voltage. Could be this a bug in eDesigner or I have missed some
other feature.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.