2017-07-31 10:11 PM
Hello all,
I'm working here with the 'L9906CB'. I have some questions regarding the functionality of the IC, which I could not clarify by looking into the datasheet (this is the only document I could get for this IC) or via other topics in the forum. The questions are: 1) The L9906 has a shoot through protection functionality. In our case, the value for the duration of the shoot through protection is always set to 100-200 ns. Until now, I had the feeling that the L9906 adds this 100-200 ns ON TOP of the dead time of my switching signals, which are the input signals for the L9906. Is that correct? Furthermore I have the question: The declaration of 100-200 ns from the datasheet still give still a range for the duration of this additional dead time. I want to quantify the real dead time, which I have in my PWM. And I don't know now, which is the value that is added exactly. Could you help me also with this issue? 2) The second point is: Using the L9906, is it possible to activate a Highside-MOSFET and/or a Lowside-MOSFET for a 'long' period of time, i.e. not to use a PWM in this time but just activate one of the switches? My concern here is, that this could affect the functionality of the Boost-Converter for the switching of the Highside-FET.... Or is this not a problem at all?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.