2013-04-17 2:53 AM
Hello, I've prototyped a led driver built around
an HVLED815PF, it's woking nicely.Now I'd like to add an integrated day/nightswitch to the lamp, with minimal components. Is it possible to put the HVLED815 in some sort of sleep-mode or standby, with minimal power consumption from th supply (while the rectified mains is still on the drain)? Or I have to disconnect the circuit formthe mains supply?The lamp is a 10W led lamp, powered from 230V mains, high power factor circuit, not dimmable, built adapting theAN4129 schematic and component values.Thanks,Fabio Eboli #hvled815 #led2013-04-22 3:10 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.