cancel
Showing results for 
Search instead for 
Did you mean: 

Power dissipation of L9960

Amrutha
Associate

Hi,

we are using L9960 H-Bridge -L9960 for automotive application.

Here are the inputs to consider using L9960.

ParametersMinTypicalMaxRemarks
Input Voltage (UBAT)8. V13.5 V18. VL9960 device will supports 4.5V > < 28V
Output Voltage (Out)7.4 V12.3 V15.75 VOutput voltage almost same due to FETs switching
Input Current (IBAT)3. mA4. mA5. mADevice current consumption for normal operation
Output Load Current (ILOAD)2. A3. A5. AL9960 device will supports 1A > ILOAD < 15A

Could you please help me with power dissipation calculation of this IC. I am aware of this application note an4867-l9960-l9960t-automotive-integrated-hbridges-stmicroelectronics.pdf . 

But can i get any worksheet for the same for doing power dissipation calculation?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Joe WILLIAMS
ST Employee

Hi Amrutha

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Kind Regards

Joe

STMicro Support

Amrutha
Associate

Sure, Thanks