2023-09-06 4:39 AM
We need PMIC for Automotive application with 24V with SPI and watchdog with ASIL D
2023-09-07 2:14 AM
Kindly reply to the above PMIC requirement
2023-09-07 4:28 AM
Welcome @SU1, to the community!
With your given parameters you can have a look at the following PMICs:
They can be operated with a VBAT of up to 32V. But you probably need a higher input voltage range because of the expected load dump tests, don't you?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.