2019-04-25 1:32 PM
I wanted to use the X-Nucleo-IHM02A1 stepper motor driver board in a project that has a 3.8 volt motor. The data sheet for the L6470, and the guide for the IHM02A1, list the Motor Supply voltage (Vs) as 8 to 45 volts. Does this mean that the L6470 is not compatible with my 3.8V motor ?
2019-04-25 2:12 PM
Yes, the motor would be compatible. Motors are inductive loads, which are current dependent. That datasheet would have also specified a current at 3.8 Volts.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.