2018-09-15 11:36 PM
I attended the excellent motor control sessions last week at the ST Developers Conference in Santa Clara, CA. At the presentation I received the Nucleo F302R8 and X-Nucleo-IHM07M1 boards which I've been experimenting with. However, I would now like to use ST Motor Control Workbench to target the STM32F429ZI chip we are looking to use in our custom motor control systems. To get started, I would like to pair the X-Nucleo-IHM07M1 with the Nucleo F429ZI development board, but I don't see a way of selecting the STM32F429ZI MCU in the Motor Control Workbench.
The closest I can get is in the "MCU and Clock Frequency Selection" is choosing "STM32F4xx" as the MCU type and "STM32F417IG" as the MCU. With this I can produce the ST32CubeMX project, but within STM32CubMX, I can't change the MCU to the actual STM32F429 MCU I would like to target.
Is there a way of using the ST Motor Control Workbench to easily target the STM32F429? Is there an alternative way of using the STM32CubeMX to manually configure a project with the Motor Control middleware and the STM32F429 MCU?
Thanks,
Mike Thompson
2018-09-17 12:48 AM
Hello Mike,
First thanks for your positive feedback on the motor control workshop in Santa Clara.
About your request, yes there is a way to use a new MCU using CubeMX.
We prepared an application note that should help you, AN5166 at the following address:
https://www.st.com/resource/en/application_note/dm00505156.pdf
Please tell us if it helps you and if you have still problems don't hesitate to contact us,
Best regards,
Claire
2018-09-21 12:49 AM
Terrific. I'll read through this and get back with any further questions.
2018-09-30 8:18 PM
OK, I've read through AN5166 and it answers a LOT of my questions. Particularly where it describes using the import feature of STM32CubeMX to import the .ioc from a motor control project to another project that has my specific chip (STM32F429) in my case. Unfortunately, I am running into other hardware issues which I'll ask under another topic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.