2016-11-05 11:04 AM
Hi
I would like to use L7987LTR in a few designs. The datasheet of the IC says its able to provide 2 A current however I can only measure 0.5 A. I have tested the schematics in 3 different layouts and layouts all seem to be good but all have the same behaviour. This makes me believe the problem is not in layout.
Moreover, I have tried a few differnet inductors (10uH) and diodes but I only measure 0.5 A output current. What am doing wrong? why does not the IC provide more current?
Thank you for you time in advance.
L2 = NR8040T100M (3.1A 2 mOhm Max ), LQH43PN100M26L, 744045100
D5 = NRVTS260ESFT1G (650mV @ 2A), B340B-13-F (500mV @ 3A)
Best regards,
-Alex
#dc-dc-conversion #l79872016-11-13 12:19 AM
2024-12-23 2:05 AM - edited 2024-12-23 2:06 AM
Change R34 to 39K.
edit: oeps...just saw it's a very old post :see_no_evil_monkey:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.