2024-11-05 9:38 PM
I am working on L6474PD motor Driver.
I could figure out that, if the input is between 8-48v it would internally regulate the voltage and supply to the logic circuit of L6474PD , but my question is will the L6474PD independently drive the stepper motor or should i externally give the supply to stepper motors
waiting for a detailed reply!!!
2024-11-06 7:12 AM
Welcome @Dhruv_Poovayaya, to the community!
I don't fully understand your question, can you please explain it in more detail, what do you mean by independent drive?
Regards
/Peter
2024-11-06 7:39 AM
Basically my question is , L6474PD motor driver is given an input between 8-48v and at the output a stepper is connected, should I external provide supply to the motor or will the L6474PD will be able to drive the stepper motor
2024-11-16 4:15 AM
Does this Motor Driver L6474PD have Internal Protection for Back EMF?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.