2015-06-22 7:05 AM
I've been encountering a strange problem. I can use the L6474 to move a stepper motor pretty fast in the forward direction. When I flip the direction bit though, I find that I can't make it move anywhere near as fast in the reverse direction. Any idea what might be causing this?
2015-07-01 4:53 AM
Hi,
How much is the speed difference? Whant is the mechanical load of the motor? Enrico2015-07-15 12:54 PM
Sorry for the late response, but I didn't see your reply earlier.
This happens even on an unloaded motor. I don't have a precise speed measurement available, but I believe that it happens at around 144000 pulses per second. I did some ad hoc changes to the firmware that seemed to mask out this problem, so I don't have any specifics on hand about the speed difference.Still, the fact that this occurs on a completely loaded motor is strange.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.