2014-06-19 10:29 PM
Hi
I'm using L6470.It works to move step motor a bit,when the Powered on.The motor's coil Voltage was high between the RESET turn high and First SPI communication is started.(Almost 10ms?CPU's order)I don't want to move a bit when the IC powered on.What is the problem about that??SW terminal is LOW when the RESET turn high. #l6470-power-on-resetWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.