2014-01-29 4:04 AM
Hy, i must use a full bridge driver L6297 for control two normal DC motor 24V.
My uP is STM32 Cortex STM32F100 with 3,3 Volt supply. Can i control direcly the L6207 with 3,3 Volt level ?? for all the signal control: In digital, enable, pwm, Vref ..... Thank you2014-02-03 2:38 AM
Hi, all the digital inputs of the L6207 are compliant with the 3.3 V logic signals and you can ajust the VREF using a 3.3 V PWM without any limitation.
Regards Enrico2014-02-03 3:43 AM
Thank you very much
Best regards MicheleWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.