2022-07-29 11:17 AM
2022-08-08 3:55 PM
Welcome, @CRAMF.1, to the community!
Yes, you can also use a polycrystalline digital potentiometer as a RILIM instead of a fixed resistor. The important thing is that it is a real ohmic resistor and not a semiconductor junction whose behaviour may not be suitable.
However, please keep an eye on the non-linear characteristic of ISKIP current vs. RILIM, so that you do not overload the IRLED.
Does it answer your question?
Regards
/Peter
2022-08-08 5:58 PM
Hi Peter,
Thank you for confirming. I was waiting for your reply before looking into the details of the resistive properties provided by digital potentiometers. If the latter do not come with ohmic output resistances then I might look at using a 1x8 multiplexer connected to a various resistances. I am currently busy with another project and I may get back to you if I have additional questions regarding the ISKIP parameter you have mentioned below. Thank you for the heads-up!
Chundra Ramful, P.Eng.
[ personal information removed by moderator ]
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.