cancel
Showing results for 
Search instead for 
Did you mean: 

How about SL-CNWLC05801V1?

Schuyler
Senior

At present, I have contacted the project about NFC power supply, but there has been no progress. The energy output through the EH pin of ST25DV has not successfully powered L4(MCU). Currently we know that SL-CNWLC05801V1 uses STM8, can its MCU be powered by NFC power supply? Is there any other way I can wirelessly power the MCU via NFC?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Peter BENSCH
ST Employee

The SL-CNWLC05801V1 is a suggestion on how to implement an NFC reader in automotive environments. However, the STM8S mentioned there is not an ultra low power MCU, so it cannot be powered by the few milliwatts from the NFC field. Instead, one could use an STM8L, where it must be noted, however, that all STM8s are set to NRND (Not recommended for new design).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Peter BENSCH 

Ok, so if I want to use the NFC antenna to get energy that can drive the MCU, how do I design the energy that I get from the NFC to charge the battery and then drive the MCU? Is this feasible?

The problem will be that batteries typically require a more or less complex charging circuit with a correspondingly high input voltage. If you can find a battery that can be charged together with the charging circuit (!) with significantly less than 10mW, this should be possible, but then not charge the battery and operate the MCU at the same time.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Schuyler
Senior

Hi @Peter BENSCH 

Well, I'm very interested in your suggestion. So does ST have a sample product with NFC antenna and battery charging?

Not that I know of.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.