cancel
Showing results for 
Search instead for 
Did you mean: 

Hello I intend to incorporate MASTERGAN1 switching at 1.000MHz with duty cycle control How well MASTERGAN1 behave at 1MHz?

AEzio.1
Associate

Hello

I intend to incorporate MASTERGAN1

as a resonance converter switching at 1.000MHz with duty cycle control from 20% to 50% [ symmetrical]

HV <=40VDC Output power up to 40Watts

How well the MASTERGAN1 behave at 1MHz?

Compared with TI LMG5200?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ken2399
Associate II

Hi,

I'm just using the evalmastergan1 board to do some double pulse tests. Working fine with 100ns pulses at 100V 8A, so I don't see a problem at 1MHz 40W.

Cheers!

0693W00000Y9kR2QAJ.png

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.