2020-05-10 11:10 PM
Hello, I am using the stm32L433Rc and a maxon motor (9 V, initial current 11,4 A, continous current 3 A). Now I am looking for a motor drive inbetween. I am thinking of using the a) VNH7100 or b) the L9960. Has any one experience with one of these? I am worried about burning the motor with a) as I cannot limit the current here and with b) that the maximum provided current could be not enough for get the motor going.
Also I am wondering whether the VNH7100 is compatible with the stm32L433RC regarding the current sense function.
Thanks for your help!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.