2018-09-04 1:32 AM
Hi, does anyone knows how to read current to motor by calling a function in SDK 5.2?
2018-09-04 5:45 AM
Hello,
Depending on what you actually want, there are two ways:
These values are expressed in S16A unit. To convert them into Amperes, use the formula displayed in the reference documentation for function MC_GetPhaseCurrentAmplitudeMotor1().
2018-09-05 9:37 AM
Hi Fred,
Where can I get the reference document you mentioned
Thanks
2018-09-18 12:04 AM
Hello Diandi,
Sorry for the late answer. The reference document is accessible from the Motor Control Workbench: in menu "Documentation", select item "Firmware Reference".
Alternatively, you can browse to the folder where the Motor Control SDK is installed (e.g. C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.2.0) and go in the "Documentation" subdirectory. There, you'll find the MotorControlSDKFirmware.chm file. Simply double-click on it and the reference documentation will open.
Best Regards,
Fred.
2019-04-17 11:14 PM
Dear Fred
if i don't call "MC_StartMotor1() " this function but just call "MC_GetIabMotor1() "
can i get the current flow to motor?
2019-05-07 11:42 PM
Hello Frank,
The current will start to flow in the motor only after MC_StartMotor1() is executed, So without this the MC_GetIabMotor1() function will only return 0.
2020-04-16 1:53 AM
Hello VSHAR
I found that the the phaseCurrent value by calling MC_GetPhaseCurrentAmplitudeMotor1() is not inaccurate during heavy load ex when climbing the hill
Is there any way to fix this problems?
2021-10-12 12:52 AM
I am an newbie in the motor control + IAR
Is there any guidance document to teach how to display current in s16a format in IAR debug mode?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.