2026-03-10 2:51 AM
Hi
In this
I want to connect this board to my STM32F767ZI, BUT Data lines D+/D- on Its USB-C Connector are not connected to any test point. Is there any workaround this? I can solder wires to for example A side of this connector(D+/D-) but then B side will be left unconnected. I can live with the fact that USB CABLE will work in only 1 orientation when inserted in USB-C Receptable but i am unsure of any other consequences that it will cause? Power delivery contracts/CC1/2, etc..
I know ST offers another Development board STEVAL-ISC005V1 where these signals are available but don't need so many Voltage Outputs and EVAL-SCS001V1 fits perfectly.
Solved! Go to Solution.
2026-03-12 1:39 AM
On the EVAL‑SCS001V1 the USB‑C connector is intended only for power‑delivery, not as a USB data port, which is why D+/D- are not brought out. In principle you can solder to one side’s D+/D- pads and accept that the plug will only work in one orientation; the CC pins handled by the STM32G0 on the board will still negotiate the PD contract, and leaving the other D+/D- pair unconnected does not affect PD itself.
However:
So: your workaround may function for lab experiments, but it is a hack and not recommended for a final design.
Hope that helps?
Regards
/Peter
2026-03-12 1:39 AM
On the EVAL‑SCS001V1 the USB‑C connector is intended only for power‑delivery, not as a USB data port, which is why D+/D- are not brought out. In principle you can solder to one side’s D+/D- pads and accept that the plug will only work in one orientation; the CC pins handled by the STM32G0 on the board will still negotiate the PD contract, and leaving the other D+/D- pair unconnected does not affect PD itself.
However:
So: your workaround may function for lab experiments, but it is a hack and not recommended for a final design.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.