cancel
Showing results for 
Search instead for 
Did you mean: 

E-L9823 pin 21 - NC

dcflipflop
Associate

Hi. Looking to use E-L9823 as a replacement in a legacy design.

The datasheet states pin 21 is not connected. Looking to confirm it is a true "no connect" internally on the part.  On our existing PCB it will be tied to +24V. Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions

I opened a case and received the following reply from ST Customer Support.  I have not tried the part in circuit yet.

"For N.C. Pins, there is absolutely no connection from the pin labeled NC to the die. So it is floating."

View solution in original post

3 REPLIES 3
Harirajan
Associate II

Hello ,

Did you find solution?  I'm also dealing with the same issue.

I opened a case and received the following reply from ST Customer Support.  I have not tried the part in circuit yet.

"For N.C. Pins, there is absolutely no connection from the pin labeled NC to the die. So it is floating."

Ok for my case, they connected it to 24V, still now no issues observed. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.