2020-01-17 1:23 AM
Can I know what is the max current rating per channel of the smart FET VNQ5050AK-E, it is quad channel IC and its total current is internally limited to 19A.
2020-01-19 12:07 AM
Do worse case design - that is calculate from maximum or minimum figures different ways then use the worse realistic figure.
For safe design assume 27A x 4. Table 9
That comes down to less than 7A per output over temperature. Less than 7A x4. Table 9. All four outputs in parallel gives less than 30A
Use the the thermal graph of 'C per watt to estimate the heatsink of your PCB depending on copper area. 55'C to 35'C per watt, graph 26. Look up the maximum on resistance and from that re-arrange from W = I squared R to find the maximum current.
You need to go through the datasheet first estimating what you want then checking and improving your estimate.
Table 6 tells you the maximum R on at different temperatures 50mR, 65mR and 100mR depending on Vcc and temperature for example. Use the worse case in your application.
2020-01-20 10:35 PM
Hello Andrew,
Thank you for your reply, it helped me in understanding a little but the Tables you are referring in your explanation should I check it in Datasheet of IC, if yes than references you have made are not matching with that of datasheet.
Thank you.
2020-01-20 11:39 PM
Yes I did make a mistake or the datasheet was a different version. I have corrected below.
Here is a link to the datasheet; https://my.st.com/resource/en/datasheet/vnq5050ak-e.pdf
Do worse case design - that is calculate from maximum or minimum figures different ways then use the worse case realistic figure.
For safety design assume 27A x 4. Table 9 --- Design the PCB power tracks to carry 110A.
That comes down to less than 7A per output over temperature. Less than 7A x4. Table 9. All four outputs in parallel gives less than 30A
Use the the thermal graph of 'C per watt to estimate the heat-sink of your PCB depending on copper area. 55'C to 35'C per watt, graph 26 Figures 26 and 29. Look up the maximum on resistance and from that re-arrange from W = I squared R to find the maximum current.
Note; Temperature rise = The device maximum working temperature - Your maximum working temperature.
You need to go through the datasheet first estimating what you want then checking and improving your estimate.
Table 6 tells you the maximum R on at different temperatures 50mR, 65mR and 100mR depending on Vcc and temperature for example. Use the worse case in your application.
2020-01-21 1:50 AM
2020-01-21 7:05 AM
Hi Raviraj,
Those things are for you to understand and work out. I was trying to get you started. Also I have not checked to see if the part is automotive grade and can withstand the voltages that may arise that is also for you to check?
Regards
Andrew
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.