cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot install firmware or drivers for STEVAL-PCC009V2 board to use eval6470pd board due to Windows error

ENovk.1
Associate II

When I run the updater, and press 'start', an error occurs during the step, "Install IBUUI drivers". The error message is

Error installing C:\Program Files(x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Updater\Drivers\WinXP\IBUUI.inf driver. Access is denied

This file is present in the location and has read access by all groups listed under the file properties. I tried to run the IBUUI Board Updater as Administrator (right-clicking on it and choosing that option) but this did not change the behavior.

I also tried the alternate procedure to use STM32 ST-LINK software as described in the dm00268136 Spinfamily evaluation tool document, however once I try to connect to the MCU target, it says "No ST-Link detected." It is difficult to believe that I'd need another piece of hardware not required for my project in order to make the hardware I purchased work, since all the documentation on the EVAL6470PD says all I need is the EVAL6470PD and the STEVAL-PCC009V2.

The environment is Windows 10, current up to date.

My apologies if this already shows up in the community forums, I'm not sure if this is the same feed.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Cristiana SCARAMEL
ST Employee

I'm sorry but the only solution is the firmware update using the ST-LInk/V2 programmer or an equivalent tool as reported in the user manual UM2020

If you feel a post has answered your question, please click "Accept as Solution"

View solution in original post

1 REPLY 1
Cristiana SCARAMEL
ST Employee

I'm sorry but the only solution is the firmware update using the ST-LInk/V2 programmer or an equivalent tool as reported in the user manual UM2020

If you feel a post has answered your question, please click "Accept as Solution"
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.